Infinity� IdealComfort� Furnace from Carrier

Introduces a Whole New Level of Comfort

INDIANAPOLIS, IND., Jan. 22, 2008 – The Infinity® IdealComfort™ System modulating gas furnace from Carrier introduces a whole new level of comfort by providing up to 3.5 times tighter temperature control than most standard furnaces, providing significant energy savings. It is also the quietest gas furnace on the market.

This two-stage furnace can remain at low speed, allowing it to automatically adjust to a desired temperature. Many consumers do not realize that although their thermostat is set to a certain temperature, the temperature can fluctuate one degree up or down causing a noticeable difference in comfort.

"With traditional furnaces, homeowners might notice a change in temperature just before their furnace turns on and just after the furnace turns off," said Allison Eckstein, Carrier's marketing manager for heating products." With the Infinity IdealComfort System, there no noticeable change because it maintains the temperature within 0.3� F of the set point."

In addition to better comfort control, the IdealComfort System furnace also offers excellent energy savings. Consumers can save up to $345 a year in energy costs versus previous Carrier single-stage models.

Eckstein added, "Unlike some variable speed products on the market, the IdealComfort System requires no special training or procedures to install. This furnace is as easy to install as any Infinity furnace in the Carrier line. Any technician who can install a two-stage gas valve unit can install an IdealComfort System furnace."

About Carrier Corporation

Carrier Corporation is the world's largest manufacturer of heating, air conditioning and refrigeration systems and equipment. It is a subsidiary of United Technologies Corporation (NYSE:UTX), provider of a broad range of high–technology products and support services to the aerospace and building systems industries.